Q&A Community - JLCPCB
Hello I need ENEPIG gold plating on the Rogers board. Can you make it?
Is the JLC04161H-2116D 4-layer stack-up option no longer available?
Do you have a detailled stack-up of a standard 4-Layer FR4 1.6mm PCB? I could not find it on your website.
https://www.youtube.com/watch?v=5V7dXCTpLK0 HOW CAN I MAKE THE RADIO PCB GERBER IN THIS VIDEO
Hii. Can i pay in chinese yuan for prototype pcb ? If yes, how can i do that ?
I have a board, where i have both TH-components and SMD on the same side, the top side. Because of that, i have chosen top......
Hello, I am about to send a manufacturing request for a PCB I designed in Altium which includes internal power planes. Pla......
I understand that JLCPCB only offers 1-layer aluminum PCB's, however, I am curious to know if you can apply 1mm vias from ......
Are your boards Conflict Mineral Compliant? If so, are there documents to prove this? Thank you.
Hello, I use KiCAD to design my PCB boards, and in parts of my design, the silkscreen overlaps with the copper pads. But K......
Hello, I am currently preparing for a project that involves very complex components like high pin count FPGA and MCU's and......
I wish to stack 2 x C3001542 using your footprint RJ45-TH_HYCW61-RJ45-152B How close can I physically have them together s......
Can you solder some wires to a PCB for power connection? Like this? the wire is 22AWG 300V Rated. 150mm length. Can I rais......
I purchased $23 worth of boards and until recently, had much cheaper shipping options. After temporary tariff changes in a......
My board, approx 33x20mm is shaped as a rectangle with a triangular section missing. Is there a cost per liner mm of cut, ......
Hello, I have designed a PCB where the clearance between traces and pins is 0.2mm (200µm). I would like to confirm if this......
I am writing an outline in KeepOutLayer, but the preview in the Gerber viewer does not seem to reflect this. I have also p......
is it possible have the pads with Enig surface finish on th bottom and HASL on the Top, on the same PCB?
I have two PCB designs, that when combined, would both fit on a stencil (360mmx200mm valid area). How would I go about hav......
Hello, is it possible manufacture golden fingers on flexible pcb for directly soldering to another board? Sample in pictur......
- 1
- 2
- 3
- 4
- 5
- 6
- 21