This website requires JavaScript.


Holiday Notice: JLCPCB factories will have a 3-day holiday from May 1st to 3rd. Orders can still be placed. The delivery date shall be postponed accordingly. Learn more>


How do I order a panel?

How do I order a panel?

When you have only one design in your PCB Gerber file and you need JLCPCB to help you duplicate multiple copies onto one panel, you can select the 'Panel By JLCPCB' option.


Simply check 'Yes' in the 'Panel By JLCPCB' section and fill in the number of rows (Y) and columns (X) of PCBs you want to place on one panel.


As shown in the image below, for example, if you set the panel configuration to 2 columns and 3 rows, we will merge 6 small PCBs into 1 large panel. If you order 10pcs PCBs, you will receive a total of 10 big panels, with each panel containing 6 PCBs, resulting in a total of 60 individual PCBs.



By default, we will add a 5mm board edge, as shown in the image below. It is a panel PCB with 2 rows and 5 columns.



Note:


Please ensure that the single PCB size is larger than 1.5cm x 1.5cm. Otherwise, a v-cut cost of $14.5 will be applied. Small PCBs are difficult to v-cut.


Based on our current production capabilities, please ensure that there are no more than 25 V-cut lines on either the X or Y side.


Please ensure that the board outline is simple. For complex board outlines, you will need to panelize them yourself.


Last updated on Apr 24, 2025