Instructions for ordering
Instructions for ordering
This description aims to explain common confusion that our users have encountered when placing orders and addresses frequent problems that have arisen in the past. It outlines the routine internal operations that JLCPCB undertakes upon receiving an order. To prevent unnecessary complications, please carefully read these instructions before placing your order.
Instructions for PCB orders
1. Solder-Resistance Bridges
To do solder-resistance bridges, usually, the spacing between the pads /pins needs to be at least 0.2mm on 1 or 2 layer board, and 0.1mm on multilayer board. Click here to check more details.
Special notes are required when ordering such as: solder mask bridge is required. Or it may be ignored easily.
2. The English Descriptions and Other Attachments in the Zip File
The English descriptions and other statements in your zip file, such as some PDF files, DXF files, excel, etc., will be disregarded and the PCB will be done according to the Gerber file provided only. So please make sure that the correct parameters are chosen and all those needed are converted into your Gerber file when you place your order. If any important, please kindly add it to the remark field when you place your order.
3. PCB File and Gerber File in the Zip File at the Same Time
If there are both PCB files and Gerber files in your zip file, we will follow the Gerber file and ignore the PCB file.
4. Plated Edges/ Slots ( no longer than 6mm)
If there is any edge plating needed, or any plated slots are needed, please make sure that is not longer than 6 mm, and make a note about it when you place your order, or we can not make it for you. If there is no any note about it, then we will make it with the normal process.
5. Issues with Software Incompatibility
Since different clients will use different software to design the board, and the software we process the Gerber data is also not the same as the software used for designing, so sometimes the software incompatibility problem arises. Since there is no warning about the issue when importing the data into the software, so we have no way to notice it and thus cannot confirm with our customers. Therefore, we are responsible for half of the order problems caused by software incompatibility.
6. Markings on Base Materials
For the sake of security, there are some markings on the base material, which are based on the base material itself, and we have no way to remove them. We have no idea about which PCB will be with such kind of markings, so your PCB will also have the chance to have the markings. Please kindly check whether it is acceptable before placing your order.
7. Designs about Slots, Cutouts, Millings and V-Cut
Please kindly make sure that the V-cut lines, cutouts, millings and slots are in the same layer with the board outline. If it is not in the same layer with the board outline, it will be missed. So please kindly check it before placing your order. If it is missed due to they are not in the same layer with the board outline, we will not be responsible for it. ( If the slots are to be plated, it needs to be with the drill holes in the same layer, or it will be missed easily).
8. Gerber View
As to the preview / Gerber Viewer on the website, it is only for the purpose of reviewing the file quickly before paying for your order. However, there may be instances where the website does not display it EXACTLY as intended, so it's advisable to carefully review your file when placing your order if you have any doubts.
9. Silkscreen/ Texts
To make the silkscreen clear on the board, the width of the texts ( filled lines) and the space between letters need to be no less than 0.15 mm with a height no less than 1 mm. The preferred ratio of width to height is 1:6. If outline font is designed and the solid part is filled with lines, then the filling line needs to be no less than 0.15mm too, and the hollow part needs to be more than 0.2mm.
Usually, we will not check and modify silkscreen in the Gerber file, but the texts may be widened into 0.15mm if it is not enough. And we may not accept the complaint regarding the unclear texts caused by non-standard design. Please kindly make sure the silkscreen meets our capability before ordering.
When the silkscreen overlaps with the openings, we will follow the principle of prioritizing the openings. In another word, we will ignore the silkscreen and make the openings on the boards only. Under the circumstances, if you want to keep the silkscreen on the openings, please kindly make a note in the remark column so that we can let our engineers and factories pay attention to it and meet your needs.
Silkscreen on Aluminum PCBs:
Currently, we support white and black silkscreen colors for Aluminum boards. White silkscreen will be applied to green and black solder mask ink while black silkscreen for white solder mask ink.
Please kindly note, silkscreen is not recommended on bare Aluminum surface due to its low level of adhesion and hence will easily fall off from the surface.
Also, the white silkscreen could not be clearly shown on the greyish white bare Aluminum surface. Please specify your request in the remark column if silkscreen on bare Aluminum surface is indeed wanted.
10. 4 Layer PCB
Basically, we don't make 3 layer PCB, if your order is a 4 layer and there is one inner layer only, we will process it with the 4 layer process directly and will confirm with you again. So please check whether there is any inner layer miss or not when you place your order.
11. About Repeat Order
Usually, the repeat order is directly produced according to the production file for your previous order, and we will not make any change to the production file anymore. So make sure you don't leave any note related to order changing when you place your order. The repeat order will no longer be manually checked by our engineers.
Note: Engineering fee will still charge by the system since our engineers need to re-panelise the boards manually.
12. About the Items in the Board Outline
Basically, the board outline is to show what your PCB looks like when it is finished. So all those need to be cut with the board outline should be added into the layer with the board outline, such as v-cut lines, slots, milling, cutouts. So please remove those unnecessary to avoid any confusion. Please notice that when both the GKO layer and GM1 layer exist in the Gerber file, our engineers will ignore the GKO layer and produce boards according to the GM1 layer. If there are GMI, GM2 or GM2, GM3, GM4 layers in the gerber file at the same time, we will use the one with the smallest number after the letter GM as the outline layer by default. For example, if there are GM2, GM3, GM4 layers in the gerber file, we will proceed according to GM2 as the outline layer and ignore GM3 and GM4.
13. About File Generated from Easyeda
Easyeda is a free online tool that we provide to design the PCB, and you can place your order on JLCPCB easily and quickly. But if there is manufacturer error due to the design error, we may not responsible for that.
14. About JLCPCB Panel
Generally, if you choose JLCPCB to panel the PCB for you when you place your order, basically, we will panel your order with V-cut, but we panel those PCB with rectangle and round shape only. If you have panelized the boards yourself but chosen "Single PCB" when ordering, the numbers of designs in the Gerber file should be no more than 5, otherwise, we may cancel this order. If "Panel by Customer" has been chosen, the number of designs in the panelized Gerber file should be no more than 10.
15. About the Remark Field
There is a remark field when you place your order so that you can leave a note in case any important information, but it is not recommended to use this option since all the order with an English note will take a longer time to get it through the audition process.
16. Boards that Larger than 200mm*250mm
About the board which larger than 200mm*250mm, since the board is so large, and we will try our best to make that. But if the good board is not enough for the quantity that you order in the website, due to huge cost of production, we will send the good boards and refund the difference to you.
17. Design Considerations for the Thickness of Board Outline, Slots, Cutouts, and Milling
Usually, we suggest our clients design a thickness of 0.15mm for the board outline, slots, cutouts, and milling. However, if the thickness of these elements exceeds 0.15mm, we will follow the center of the line to create the board outline, cutouts, and milling.
18. Boards Within or Equals to 50mm*50mm
For small boards within or equal to a size of 50mm x 50mm, milling them perfectly during the milling process can be challenging due to their small size. To mitigate this issue, we often recommend panelizing the small boards.
19. Solder Mask Layer
The solder mask layer is normally a must layer. Please make sure you have included it in your Gerber file. If the solder mask layer is not found, or the solder mask layer is blank, the board will be made as fully covered by solder mask ink as default. So please design the solder mask layer correctly if you want solder mask opening. And if you want the full board to be covered by tin, please remember to remark it when ordering.
20. About Plated Slots
For a plated slot, the length of it should be twice larger than the width of it. The slot may have problems if it is not designed according to this. And the setting of the length and width of the slot needs to be correct as well.
Other instructions:
1. About Order Cancellation
For those order that there are some layers missed, such as no board outline and drilling, we will cancel the order directly. If there is no drill needed, etc, you had better to make a note about it when placing your order, or it will be canceled directly during the audit process.
2. Orders Beyond Our Capabilities
For orders that exceed our capabilities, we will cancel the order directly and will send an e-mail to inform you of the reasons. So please kindly check your file carefully before making payment to avoid losses resulting from the cancellation.
3. About Stencil Production File
Basically, you choose JLCPCB to panelize the PCB for you, if there is no stencil order with, we will not make the production file for the stencil since the engineers who make the production file do not know how to make the production file for the stencil.
4. Removing Order Numbers:
For orders that choose the 'Remove Order Number' service or specify a location service, we typically follow the clients' instructions when manufacturing the boards. Just in case, we also suggest clients to choose Confirm Production File service which allows for double-checking.
Generally, it will not affect the function of the boards if JLCPCB miss to remove the order number or put it by random, in this case, we will refund the remove order number fee.
Instructions for Stencil order
1. Solder paste layer is highly recommended to include in the Gerber file.
A paste layer will be much helpful in making the production file. And once your file includes a solder paste layer, your stencil will be made based on it. So please ensure that it contains all required elements.
Note:
For items which are on the solder mask layer but not on solder paste layer, an engineering question will be raised to confirm with you. If you don't want this engineer question, you may leave an ordering remark“Please follow the solder paste layer only, and ignore the difference between the solder mask layer and solder paste layer.”
2. Apertures processing standard
As default, apertures such as IC, BGA, and capacitor/resistor of footprint 0805 and above, will be processed as default standard. If you don't need it processed as the standard, or want apertures to be exactly the same as your paste layer, please leave a remark.
Please refer to this link for our standard details of aperture processing. https://jlcpcb.com/help/article/opening-process-standard-of-stencil.
3. Stencil Thickness
There is an option of stencil thickness for you to choose from on the ordering page. You can either select a thickness by yourself, or you can just let JLCPCB engineer to select the appropriate thickness for you based on your Gerber file features.
We offer standard thickness options for free of 0.1, 0.12, 0.15, 0.18, and 0.2 mm. And special thicknesses of 0.03, 0.04, 0.05, 0.06, 0.08, 0.25, 0.3, 0.4, and 0.5 mm are available at an additional cost.
4. Valid area
The valid area of the stencil is the part where laser cutting can be processed, for both the stencil apertures and custom size.
Basically, the valid area for frame stencil is the area within the adhesive tape on back side. While for non-frame stencil, it is the area excluding that taken by the clamping device when machining, which is about 8mm on one direction. For details, please referring to the ordering option of Dimensions.
5. Customized size
If you request a custom size of a non-frame stencil, please select Yes for the 'Customized size' option. And please make sure that the custom size is within the valid area of the stencil.
6. Fiducials
If fiducials are required, please ensure that you select the 'Etched Through' or 'Etched Half' option for option 'Fiducials' and include the fiducials design in the file as well. If any inconsistency between option and design, fiducials will not be made on the stencil.
7. Stencil side of 'Top+Bottom(On Single Stencil)’
If you request the stencil side to be 'Top+Bottom(On Single Stencil)', it means that the stencil valid area should be larger than double size of the PCB. So please select the suitable dimension for the stencil to proceed correctly.
8. Panel stencil
A panel stencil is supported. If the PCB is 'Panel by JLCPCB', the stencil will also be panel accordingly.
It is also supported that customer has several designs in one paste layer, or simply combine several paste layers in one folder for JLCPCB to panel for you. Please kindly leave a stencil remark for better understanding. And please note that some of the situations may require an extra cost according to the specific cases below: https://jlcpcb.com/help/article/in-what-cases-will-there-be-charged-extra
9. About typesetting for different designs in your stencil file
Some stencils may have more than one designs on single stencil.
Generally, if the stencil size is large enough to accommodate different designs, we will not alter the typesetting of your designs (for two or more designs within the same stencil file). However, if the stencil size is insufficient, we may adjust the typesetting of designs to ensure they fit on the stencil. If no changes are allowed for the typesetting, please leave a remark when placing your order.
10. About the Stencil Orientation
Generally, if there is no specific note regarding the placement or direction of the cutout on the stencil, the long side of the PCB will automatically align with the long side of the stencil.
11. Packages for nor-frame and frame stencil.
1) For non-frame stencil less than 25*25cm, it will be put in the plastic bag and then packed in flight case.
While over 25*25cm, it will be put in two wood plates first and then packed in cardboard box.
2) For frame stencils of all dimension, they will be put in the cardboard box with wood plates outside for protection.
Other instruction
Complaints about Reorder Orders
Please kindly check or test the order upon receipt. If any issues are found and confirmed to be due to JLCPCB's error, we will offer a refund or remake the order. If no feedback is provided and the order is placed again, any issues with the initial order and the reorder will only be covered for the first order.
Last updated on Apr 19, 2025