Blog - JLCPCB
Blind vs Buried Vias: A Comprehensive Guide for PCB Design
A printed circuit board (PCB) is made up of layers of copper foil circuits stacked on top of each other, and the connections between different circuit layers rely on vias. If the holes drilled by a drilling machine or laser are left as is, they will not conduct electricity, because the surface of the original drilled hole is only resin, which is not conductive. Therefore, a layer of conductive material (usually copper) must be plated on the surface of the drilled hole. In this way, current propagates ......
Apr 22, 2025
- 1
- 2
- 3
- 4
- 5
- 6
- 7