This website requires JavaScript.


Holiday Notice: JLCPCB factories will have a 3-day holiday from May 1st to 3rd. Orders can still be placed. The delivery date shall be postponed accordingly. Learn more>


How Laser-Made PCBs Are Used in Rapid Prototyping

Blog  /  How Laser-Made PCBs Are Used in Rapid Prototyping

How Laser-Made PCBs Are Used in Rapid Prototyping

Apr 21, 2025

In the fast-paced world of electronics development, rapid prototyping is crucial for reducing design cycles and bringing products to market quickly. Traditional PCB fabrication methods can be time-consuming and costly, especially for small batches or prototype designs. There are many methods to prepare a PCB at home in a professional way, some of them require chemical processes and photolithographic steps. The other methods are not so handy and need bigger machines. However, advancements in laser technology have revolutionized PCB prototyping, offering faster turnaround times and enhanced precision. Lasers can be controlled to perform many different steps in the PCB manufacturing. For example:


  • Laser Engraving: Selectively removing copper to create circuit traces.
  • Laser Cutting: Precisely cutting PCB substrates to desired shapes and sizes.
  • Laser Drilling: Creating microvias and holes with extreme accuracy.


These techniques enable engineers to create high-resolution circuit patterns quickly, making them ideal for rapid prototyping. In this article, we explore how laser-made PCBs are used in rapid prototyping, their advantages, and the best practices for implementing them in your design process. Let's discuss all the steps in detail, and to know more about PCB manufacturing see our recent article on "How PCBs are made in JLCPCB factory".


The Rise of Laser Technology in PCB Fabrication:


Laser technology has emerged as a game-changer in PCB prototyping, offering several advantages over traditional methods:


1. Precision and Accuracy: Can achieve tolerances down to a few microns.


2. Speed: Capable of creating functional PCBs in as little as 25 minutes.


3. Flexibility: Lasers can work with a variety of materials, including FR1, FR4, and flex.


4. Non-contact Processing: It is a non-contact method, eliminating mechanical stress on the board.


Laser Processes in a PCB Design:


  • Lasers Marking in PCBs
  • Lasers Cutting in PCBs
  • Lasers Sintering in PCBs
  • Lasers Drilling in PCBs


Lasers Marking in PCBs:


Lasers are also very fast when it comes to marking PCBs. They can etch codes in a few seconds while preventing the material around the area of application from any damage or distortion. Laser marking also provides information in the manufacturing of integrated circuits. In this application, precision, efficiency, and precision are very important.


laser engraving


Traditionally, identifying marks are done alphanumerically, but there are restrictions due to the space available on the PCB surface. That is why lasers are used in marking PCBs since they can offer accurate marking.


Lasers Cutting in PCBs:


Cutting is an important aspect of PCB production since a circuit board requires to be designed using a stencil with apertures to connect and solder components. A fiber laser can be used to cut PCB stencils in large volumes within a few seconds. The beam of a laser cut PCBs can punch through the circuit board material to leave the necessary apertures thereby ensuring that it doesn't compromise the integrity of the material surrounding it.


laser engraver


In the case of mass production, this process has to be done repeatedly. CNC laser PCB prevents damages from occurring and minimizes waste since they use a non-contact approach to cut materials. The cut width can be exceptionally narrow at 0.0001 inch. The dimensional accuracy is 0.0005 inches.


Lasers Sintering in PCBs:


Sintering is considered the perfect solution to affixing components of PCBs and this method can overcome the problems of soldering and enable more durable, stronger, and consistent bonds to form during the manufacturing of PCBs.


Laser sintering is giving opportunity for the development of cutting edge PCBs which are created without solder. High-density circuits are suitable for this technique, allowing improved stability. When sintering is done, a laser is applied to a powder that contains silver. The heat coming from the laser makes the powder reach a melting point and this is allowed to cool off to form a solid connection.


Lasers Drilling in PCBs:


Laser drilling makes holes on a printed-circuit-board to create connections between several layers. The electronic appliances we have in our homes consist of HDI boards that make use of laser drills. Laser drilling procedures guarantee accuracy even when working with small sizes.


laser drilling

Laser drilling utilizes laser energy for drilling a hole. This is totally different from drilling holes with a machine. Holes are drilled on PCBs for placing components and bringing interconnection between various layers. Lasers are capable of drilling between 2.5 to 3-mil vias on flat reinforced glass. It can drill about 1-mil vias when it comes to an unreinforced dielectric.


The Laser-Made PCB Prototyping Design Flow:


The process of creating laser-made PCBs for rapid prototyping typically involves the following steps:


Step 1 - Design: Engineers create the PCB layout using CAD software.


Step 2 - Laser Engraving & Etching: A fiber laser, such as the xTool F1 Ultra, precisely ablates copper, creating the circuit traces.


laser engraving


Step 3 - Hole Drilling: The laser drills holes for components and vias with high accuracy.


Step 4 - Solder Mask Application: A laser can be used to selectively remove solder mask material, exposing pads and creating a professional finish.


Step 5 - Board Cutting: Finally, the laser cuts out the board shape, completing the physical prototype.


Step 6 - Laser Sintering: In advanced PCB prototyping, a laser sinters conductive inks or metal powders to form conductive traces.


Choosing the Right Laser Source:


It is important you determine the appropriate laser source for your depaneling needs. CO2 and UV lasers have their disadvantages and advantages.


uv and co2 laser


UV lasers and CO2 Lasers:


Lasers that involve UV use “cold” cutting technology. UV lasers make it easy to control the thermal charring of the edge. Therefore, a UV laser is a better option if reducing char is more vital than speed. On the other hand a CO2 laser is a preferable option if cycle time is very important. CO2 laser PCB can help to make full cuts and are more commonly used to create perforated cuts. Making use of the perforation technique helps to reduce char and as well as allows for easier load and unload of panels and boards from the cutting machine.


uv vs co2 laser


Furthermore, the amount of charring and cycle time increases as material thickness increases. If V-grooves can be used to manufacture panels at cut locations, laser cuts can be faster and cleaner.


Factors to Consider During Laser Operations:


Some factors need to be considered during laser drilling, these two major factors should be considered;


The Copper thickness: The lowest thickness of the target copper layer should be twice as thick as the top copper layer to be drilled. Lasers are the most effective way to make microvias in PCBs. Laser-drilled microvias are important in the manufacturing of PCBs


Non-homogeneity of the stack-up: While using lasers to drill, the non-homogeneity of the stack-up is very important. Several materials get energy at various rates. For instance, FR4 resin takes up energy at the exact rate as the glass fibers. BT epoxy resin vaporizes at a much faster rate than glass and as such, leaves glass fibers in the hole.


Challenges and Considerations:


While laser-made PCBs offer numerous advantages, there are some challenges to consider. High-quality laser systems can be expensive, though they often pay for themselves in time and cost savings. Operators need training to effectively use laser systems and optimize designs for laser fabrication. Some specialized PCB materials may not be suitable for laser processing.


Conclusion:



Lasers are important and specialized equipment used in the manufacturing of PCBs. These equipment are used for several purposes, they are used for drilling, cutting, marking, and sintering PCBs. Since it offers precision, this equipment is a preferable option for PCB manufacturers. Lasers also utilize the no-contact approach making it easy to use in the production of PCBs. Laser engrave PCB is used in PCB production. Having a laser machine at home guarantees you faster prototyping in a professional way.